Hi,
Im trying to use Terminal to communicate with the CC2540, and i used the code provided from btool to send the hex files.
For example to initiate de Gap_Device in BTool i get this:
[2] : <Tx> -
-Type : 0x01 (Command)
-Opcode : 0xFE00 (GAP_DeviceInit)
-Data Length : 0x26 (38) byte(s)
ProfileRole : 0x08 ( Central )
MaxScanRsps : 0x05 (5)
IRK : 00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00
CSRK : 00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00
SignCounter : 0x00000001 (1)
Dump(Tx):
01 00 FE 26 08 05 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 01 00 00 00
So i send the "01 00 FE 26 08 05 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 01 00 00 00" in Terminal to the device but i don't get any answer.
It would be great if someone could help me and explain what am i doing wrong.
Thanks