Other Parts Discussed in Thread: CC2540
On a post here in this forum, I have noticed that a user has been able to set-up their IAR IDE so that an output window shows debug output as their code is run to a break-point.
See: http://e2e.ti.com/support/wireless_connectivity/f/538/p/349177/1222858.aspx#1222858
I think this is a very useful tool for debugging and I would like to do the same.
Can anyone advise how I could set-up my IAR IDE to do this, please.
There appears to be the need to 'Configure Tools'. However, I don;t know what I need to add to my Menu-Content or Command field therein.
I'm using IAR IDE 8.20 and developing a BLE Peripheral application with the TI CC2540 device.
Thank you.
Here's what I mean....
"Here is a snippet of my debug output on the Peripheral:
|
1
2
3
4
5
6
7
8
9
|
[simpleBLEPeripheral.c:748] USER: Peripheral State (0x1): Initialized [simpleBLEPeripheral.c:751] USER: BLE Address: 0x1CBA8C1C6A62 [simpleBLEPeripheral.c:1418] FLOW: Received a 'Connection Change' Request [simpleBLEPeripheral.c:1421] FLOW: --> Connect: 0x1 [simpleBLEPeripheral.c:1425] FLOW: Enabling Advertisements (Count 0x12c0) [simpleBLEPeripheral.c:786] Peripheral State (0x2): Advertising [simpleBLEPeripheral.c:823] Peripheral State (0x5): Connected [simpleBLEPeripheral.c:914] Pairing State (0x0): Pairing Started [simpleBLEPeripheral.c:918] --> Status (0x0): 'SUCCESS' |
Here is a snippet of my debug output on the Central:
|
1
2
3
4
5
6
7
8
9
10
11
|
[simpleBLECentral.c:677] USER: Central Device Initialized [simpleBLECentral.c:680] USER: BLE Address: 0x1CBA8C1C760A [DeviceConfig.h:372] USER: Device Filter has been Enabled [DeviceConfig.h:377] USER: --> Requested Device Filter: '0x1CBA8C1C6A62' [simpleBLECentral.c:1339] FLOW: Received a 'Connection Change' Request [simpleBLECentral.c:1342] FLOW: --> Connect: 0x1 [simpleBLECentral.c:1490] Connecting to '0x1CBA8C1C6A62' [simpleBLECentral.c:962] Pairing State (0x0): Pairing Started [simpleBLECentral.c:966] --> Status (0x0): 'SUCCESS' [simpleBLECentral.c:796] Central Event (0x5): Connection Established (Handle 0x0) [simpleBLECentral.c:799] USER: Connected to '0x1CBA8C1C6A62' |