This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Are UUID's legally protected from spoofing?

Are customer created 128 UUIDs protected legally? For example, if we wanted to create a feature and limit it to only those devices that connect to our device and have our "super sauce" UUID,in their GATT table,  is that enough legal protection? I know hackers would be able to get around this, but looking more for high volume clone prevention.

Are there other options to consider, such as just a characteristics that reads "Copyright Super Sauce..". or perhaps a certificate based system?

Thanks,

-Greg

  • Welcome to the forum Greg :)

    I don't know unfortunately and this is probably more of a question for BT SIG. From a BT core spec standpoint any device can use any 128-bit UUID, though if you use a purchased 16-bit UUID or 32-bit UUID (I'm not sure whether BT-SIG has created a purchase program for 32-bit UUIDs yet, but I imagine they will at some point) and someone were to clone it then they would be violating BT SIG rules/specs, which has legal implications to it.

  • Thanks Mr. Willis  :)