I have a problem with the temperature sensor, when I locate it in a refrigerator and the temperature drops to 0 degrees, the sensor sends the temperature measurement with intervals of +500 degrees Celsius.
The device will vacuum packaging to prevent moisture but is an error with the measurement of temperature
This sample of lectures
| +509.34 |
| +509.16 |
| +509.00 |
| +508.81 |
| +508.81 |
| +509.72 |
I'm developing a project for cold chain traceability and sensor faults is presented to me, because I need the sensor always this inside a refrigerator in a truck going to monitor the temperature