HI,
I need to develop a card that have Bluetooth 2.1 to make it device that has 2 main operations simultaneously:
1) to be connected to phone application by Bluetooth 2.1.
2) to be able to handle serial (UART) communication with Computer.
which MCU & Bluetooth 2.1 chip can I use to achieve this?
so which Kit to use and with a free Development tool (CodeComposer for example if it is possible).
Thanks.