This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2541 key fob in Network processor mode

Other Parts Discussed in Thread: CC2541, CC2540

Hi,

I need to connect a cc2541 to my MSP430 board. In fact, I am gonna use cc2541 in network processor mode. According to: http://processors.wiki.ti.com/index.php/CC254X_WITH_EXT_MCU, I need UATR/SPI. now I am wondering if cc2541 key fob already has free UART/SPI pin or I should  buy CC2541EMK?

An also for programming CC2541EMK,  CC debugger is enough or I need to buy SmartRF05EB from the CC2540 Development Kit (CC2540DK) as well?

Thanks