Hi,
I am using cc2541- Keyfobdemo to my project.
I need to save power during advertisement.
Here i am attached image which is carrying the information of current advertisement.
1. Red circle shows current advertising power.
2. Green line shows current voltage consuming by advertising (Here i need to reduce).
3. Again the other two circles shows 100 mV and 250 ms, Which means the ratio of current power taking.
My Requirements:
I need reduce the Power of Advertising- without changing advertising interval.
Tried methods:
1.
{
int8 initialTxPowerLevel = 0;
ProxReporter_SetParameter( PP_TX_POWER_LEVEL, sizeof ( int8 ), &initialTxPowerLevel );
}
2. HCI_EXT_SetTxPowerCmd( HCI_EXT_TX_POWER_MINUS_0_DBM );
3. HCI_EXT_SetTxPowerCmd( HCI_EXT_TX_POWER_MINUS_6_DBM );
4. HCI_EXT_SetTxPowerCmd( HCI_EXT_TX_POWER_MINUS_26_DBM );
5. PP_DEFAULT_TX_POWER
6. And i am using 1285ms advertising interval for maximum and minimum.
After this modification transmit power got changed during connection.
But Still i am unable to change the transmit power of advertising.
I welcome you all yours suggestions to solve this problem.
Best wishes with thanks,