This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2540/1 ADC internal reference as input channel



Is it possible to select the internal voltage reference as an input to the ADC and use AIN7, AIN6-AIN7, or AVDD5 as the reference? Channel 13 is listed as reserved, however in the BLE stack the hal_adc.h shows channel 13 as Vref.

It would be hugely useful if this configuration is possible. This would provide a way to calibrate the voltage reference. As well as enabling high-side voltage measurements that don't need resistive dividers to bring the measurements down to the reference level.

I'm guessing if this is possible it is undocumented and totally not supported.

-Mark