Hi,
I have product who sends text data through his RS-232 port.
if you connect it to PC and use terminal (for example tera-term) with the correct configuration you can send and receive data.
Baud rate: 38400
Data: 8 bit
Parity: none
Stop: 1 bit
Flow control: none
Ive connected this product with RS-232 to Ethernet converter, set the IP of server I want it to connect to and it works fine.
What im looking for is to connect to this product via BT low power, and to control it (for example talk with one of the terminals in the Android play store)
I tried to look for a solution but I think Im missing something, could be you dont have the complete solution
What are my options in this case?
If more information is needed please let me know.
Thanks for the help