All, Urgent!
We have issues to pair with TIDA00096 which is based on cc2451 chip set. the following is the response when trying to pair with cc2540 USB dongle from cc2541mini kit.
the pairing lost connection after less than 1mins. We were able to use Nokia WP8.1 phone to pair with it, the same thing happened that connection lost after less than 1mins.
also the ECG IOS APP is anot able to find the bluetooth device(cc2541).
Any input is appreciated. -Kevin
[1] : <Tx> - 08:27:42.299 -Type : 0x01 (Command) -Opcode : 0xFE09 (GAP_EstablishLinkRequest) -Data Length : 0x09 (9) byte(s) HighDutyCycle : 0x00 (Disable) WhiteList : 0x00 (Disable) AddrTypePeer : 0x00 (Public) PeerAddr : 52:06:18:16:4A:54 Dump(Tx): 01 09 FE 09 00 00 00 52 06 18 16 4A 54 ------------------------------------------------------------------------------------------------------------------------
[2] : <Rx> - 08:27:42.330 -Type : 0x04 (Event) -EventCode : 0xFF (HCI_LE_ExtEvent) -Data Length : 0x06 (6) bytes(s) Event : 0x067F (GAP_HCI_ExtentionCommandStatus) Status : 0x00 (Success) OpCode : 0xFE09 (GAP_EstablishLinkRequest) DataLength : 0x00 (0) Dump(Rx): 04 FF 06 7F 06 00 09 FE 00 ------------------------------------------------------------------------------------------------------------------------
[3] : <Tx> - 08:27:47.926 -Type : 0x01 (Command) -Opcode : 0xFD8A (GATT_ReadCharValue) -Data Length : 0x04 (4) byte(s) ConnHandle : 0x0000 (0) Handle : 0x0001 (1) Dump(Tx): 01 8A FD 04 00 00 01 00 ------------------------------------------------------------------------------------------------------------------------
[4] : <Rx> - 08:27:47.973 -Type : 0x04 (Event) -EventCode : 0xFF (HCI_LE_ExtEvent) -Data Length : 0x06 (6) bytes(s) Event : 0x067F (GAP_HCI_ExtentionCommandStatus) Status : 0x02 (Invalid Parameter) OpCode : 0xFD8A (GATT_ReadCharValue) DataLength : 0x00 (0) Dump(Rx): 04 FF 06 7F 06 02 8A FD 00 ------------------------------------------------------------------------------------------------------------------------
[5] : <Tx> - 08:27:55.022 -Type : 0x01 (Command) -Opcode : 0xFD92 (GATT_WriteCharValue) -Data Length : 0x06 (6) byte(s) ConnHandle : 0x0000 (0) Handle : 0x0048 (72) Value : 01:00 Dump(Tx): 01 92 FD 06 00 00 48 00 01 00 ------------------------------------------------------------------------------------------------------------------------
[6] : <Rx> - 08:27:55.178 -Type : 0x04 (Event) -EventCode : 0xFF (HCI_LE_ExtEvent) -Data Length : 0x06 (6) bytes(s) Event : 0x067F (GAP_HCI_ExtentionCommandStatus) Status : 0x02 (Invalid Parameter) OpCode : 0xFD92 (GATT_WriteCharValue) DataLength : 0x00 (0) Dump(Rx): 04 FF 06 7F 06 02 92 FD 00 ------------------------------------------------------------------------------------------------------------------------
[7] : <Info> - 08:28:03.852 Device Connected Handle = 0x0000 Addr Type = 0x00 (Public) BDAddr = 54:4A:16:18:06:52 ------------------------------------------------------------------------------------------------------------------------
[8] : <Rx> - 08:28:03.820 -Type : 0x04 (Event) -EventCode : 0xFF (HCI_LE_ExtEvent) -Data Length : 0x13 (19) bytes(s) Event : 0x0605 (GAP_EstablishLink) Status : 0x00 (Success) DevAddrType : 0x00 (Public) DevAddr : 54:4A:16:18:06:52 ConnHandle : 0x0000 (0) ConnInterval : 0x0050 (80) ConnLatency : 0x0000 (0) ConnTimeout : 0x07D0 (2000) ClockAccuracy : 0x00 (0) Dump(Rx): 04 FF 13 05 06 00 00 52 06 18 16 4A 54 00 00 50 00 00 00 D0 07 00 ------------------------------------------------------------------------------------------------------------------------
[9] : <Tx> - 08:28:09.368 -Type : 0x01 (Command) -Opcode : 0xFD92 (GATT_WriteCharValue) -Data Length : 0x06 (6) byte(s) ConnHandle : 0x0000 (0) Handle : 0x0048 (72) Value : 01:00 Dump(Tx): 01 92 FD 06 00 00 48 00 01 00 ------------------------------------------------------------------------------------------------------------------------
[10] : <Rx> - 08:28:09.400 -Type : 0x04 (Event) -EventCode : 0xFF (HCI_LE_ExtEvent) -Data Length : 0x06 (6) bytes(s) Event : 0x067F (GAP_HCI_ExtentionCommandStatus) Status : 0x00 (Success) OpCode : 0xFD92 (GATT_WriteCharValue) DataLength : 0x00 (0) Dump(Rx): 04 FF 06 7F 06 00 92 FD 00 ------------------------------------------------------------------------------------------------------------------------
[11] : <Rx> - 08:28:09.571 -Type : 0x04 (Event) -EventCode : 0xFF (HCI_LE_ExtEvent) -Data Length : 0x0A (10) bytes(s) Event : 0x0501 (ATT_ErrorRsp) Status : 0x00 (Success) ConnHandle : 0x0000 (0) PduLen : 0x04 (4) ReqOpcode : 0x12 (ATT_WriteReq) Handle : 0x0048 (72) ErrorCode : 0x01 (INVALID_HANDLE) : The Attribute Handle Given Was Not Valid On This Server. Dump(Rx): 04 FF 0A 01 05 00 00 00 04 12 48 00 01 ------------------------------------------------------------------------------------------------------------------------
[12] : <Tx> - 08:28:13.806 -Type : 0x01 (Command) -Opcode : 0xFD8A (GATT_ReadCharValue) -Data Length : 0x04 (4) byte(s) ConnHandle : 0x0000 (0) Handle : 0x0001 (1) Dump(Tx): 01 8A FD 04 00 00 01 00 ------------------------------------------------------------------------------------------------------------------------
[13] : <Rx> - 08:28:13.838 -Type : 0x04 (Event) -EventCode : 0xFF (HCI_LE_ExtEvent) -Data Length : 0x06 (6) bytes(s) Event : 0x067F (GAP_HCI_ExtentionCommandStatus) Status : 0x00 (Success) OpCode : 0xFD8A (GATT_ReadCharValue) DataLength : 0x00 (0) Dump(Rx): 04 FF 06 7F 06 00 8A FD 00 ------------------------------------------------------------------------------------------------------------------------
[14] : <Rx> - 08:28:13.978 -Type : 0x04 (Event) -EventCode : 0xFF (HCI_LE_ExtEvent) -Data Length : 0x08 (8) bytes(s) Event : 0x050B (ATT_ReadRsp) Status : 0x00 (Success) ConnHandle : 0x0000 (0) PduLen : 0x02 (2) Value : 00 18 Dump(Rx): 04 FF 08 0B 05 00 00 00 02 00 18 ------------------------------------------------------------------------------------------------------------------------
[15] : <Tx> - 08:28:23.105 -Type : 0x01 (Command) -Opcode : 0xFDB4 (GATT_ReadUsingCharUUID) -Data Length : 0x08 (8) byte(s) ConnHandle : 0x0000 (0) StartHandle : 0x0001 (1) EndHandle : 0xFFFF (65535) Type : 00:2A Dump(Tx): 01 B4 FD 08 00 00 01 00 FF FF 00 2A ------------------------------------------------------------------------------------------------------------------------
[16] : <Rx> - 08:28:23.152 -Type : 0x04 (Event) -EventCode : 0xFF (HCI_LE_ExtEvent) -Data Length : 0x06 (6) bytes(s) Event : 0x067F (GAP_HCI_ExtentionCommandStatus) Status : 0x00 (Success) OpCode : 0xFDB4 (GATT_ReadUsingCharUUID) DataLength : 0x00 (0) Dump(Rx): 04 FF 06 7F 06 00 B4 FD 00 ------------------------------------------------------------------------------------------------------------------------
[17] : <Rx> - 08:28:23.293 -Type : 0x04 (Event) -EventCode : 0xFF (HCI_LE_ExtEvent) -Data Length : 0x1C (28) bytes(s) Event : 0x0509 (ATT_ReadByTypeRsp) Status : 0x00 (Success) ConnHandle : 0x0000 (0) PduLen : 0x16 (22) Length : 0x15 (21) Handle : 0x0003 Data : 42:6C:6F:6F:64:50:72:65:73:73:75:72:65:20:53:65: 6E:73:6F Dump(Rx): 04 FF 1C 09 05 00 00 00 16 15 03 00 42 6C 6F 6F 64 50 72 65 73 73 75 72 65 20 53 65 6E 73 6F ------------------------------------------------------------------------------------------------------------------------
[18] : <Rx> - 08:28:23.480 -Type : 0x04 (Event) -EventCode : 0xFF (HCI_LE_ExtEvent) -Data Length : 0x06 (6) bytes(s) Event : 0x0509 (ATT_ReadByTypeRsp) Status : 0x1A (The Procedure Is Completed) ConnHandle : 0x0000 (0) PduLen : 0x00 (0) Dump(Rx): 04 FF 06 09 05 1A 00 00 00 ------------------------------------------------------------------------------------------------------------------------
[19] : <Info> - 08:28:30.571 Device Disconnected Handle = 0x0000 Addr Type = 0x00 (Public) BDAddr = 54:4A:16:18:06:52 ------------------------------------------------------------------------------------------------------------------------
[20] : <Rx> - 08:28:30.571 -Type : 0x04 (Event) -EventCode : 0xFF (HCI_LE_ExtEvent) -Data Length : 0x06 (6) bytes(s) Event : 0x0606 (GAP_TerminateLink) Status : 0x00 (Success) ConnHandle : 0x0000 (0) Reason : 0x13 (Peer Requested) Dump(Rx): 04 FF 06 06 06 00 00 00 13 ------------------------------------------------------------------------------------------------------------------------