Other Parts Discussed in Thread: MSP430F5438A
Hi,
I am trying to compile SPP demo stack using MSP GCC compiler and i see lot of issues which i don't see when using TI's compiler.
1. Firstly, when i import project, i see lot of include directories are not included (This is common for both TI and MSP GCC compiler). Is this expected or am i missing something here?
2. If i include all directories of missing header files, i see ton's of errors as follows. But the same error is not seen when using TI's compiler? Again am i missing something here.
In fact i see same kind of behavior when i try to compiler A2DP demo.
Description Resource Path Location Type
unknown type name '__SIZE_T_TYPE__' SPPDemo line 69, external location: C:\ti\ccsv6\tools\compiler\msp430_4.3.3\include\stdio.h C/C++ Problem
unused variable 'dummy' [-Wunused-variable] HCITRANS.c /SPPDemo line 531 C/C++ Problem
'RxInIndex' defined but not used [-Wunused-variable] HAL.c /SPPDemo/MSP430_EXP5438 line 87 C/C++ Problem
conflicting types for built-in function '__bis_SR_register_on_exit' SPPDemo line 103, external location: c:\ti\ccsv6\ccs_base\msp430\include_gcc\in430.h C/C++ Problem
expected '=', ',', ';', 'asm' or '__attribute__' before 'void' HAL.c /SPPDemo/MSP430_EXP5438 line 1084 C/C++ Problem
macro "_get_SR_register" passed 1 arguments, but takes just 0 SPPDemo line 50, external location: C:\ti\ccsv6\tools\compiler\msp430_4.3.3\include\intrinsics.h C/C++ Problem
expected identifier or '(' before '{' token SPPDemo line 107, external location: c:\ti\ccsv6\ccs_base\msp430\include_gcc\in430.h C/C++ Problem
ignoring #pragma vector [-Wunknown-pragmas] HAL.c /SPPDemo/MSP430_EXP5438 line 1029 C/C++ Problem
expected '=', ',', ';', 'asm' or '__attribute__' before 'void' HAL.c /SPPDemo/MSP430_EXP5438 line 1019 C/C++ Problem
expected identifier or '(' before '{' token SPPDemo line 121, external location: c:\ti\ccsv6\ccs_base\msp430\include_gcc\in430.h C/C++ Problem
ignoring #pragma vector [-Wunknown-pragmas] HAL.c /SPPDemo/MSP430_EXP5438 line 1083 C/C++ Problem
expected identifier or '(' before 'unsigned' SPPDemo line 57, external location: C:\ti\ccsv6\tools\compiler\msp430_4.3.3\include\intrinsics.h C/C++ Problem
expected '=', ',', ';', 'asm' or '__attribute__' before 'void' HAL.c /SPPDemo/MSP430_EXP5438 line 1030 C/C++ Problem
expected identifier or '(' before '{' token SPPDemo line 92, external location: c:\ti\ccsv6\ccs_base\msp430\include_gcc\in430.h C/C++ Problem
expected identifier or '(' before '__asm__' SPPDemo line 72, external location: c:\ti\ccsv6\ccs_base\msp430\include_gcc\in430.h C/C++ Problem
ignoring #pragma vector [-Wunknown-pragmas] HAL.c /SPPDemo/MSP430_EXP5438 line 1018 C/C++ Problem
conflicting types for built-in function '__bic_SR_register_on_exit' SPPDemo line 102, external location: c:\ti\ccsv6\ccs_base\msp430\include_gcc\in430.h C/C++ Problem
expected identifier or '(' before '__asm__' SPPDemo line 77, external location: c:\ti\ccsv6\ccs_base\msp430\include_gcc\in430.h C/C++ Problem
gmake: *** [HCITRANS.o] Error 1 SPPDemo C/C++ Problem
gmake: *** [Main.o] Error 1 SPPDemo C/C++ Problem
fatal error: SS1BTVS.h: No such file or directory SPPDemo line 19, external location: C:\ti\Connectivity\CC256X BT\CC256x MSP430 Bluetopia SDK\v1.5 R2\MSP430_Experimentor\Samples\SPPDemo\Main.h C/C++ Problem
unknown type name '__SIZE_T_TYPE__' SPPDemo line 57, external location: C:\ti\ccsv6\tools\compiler\msp430_4.3.3\include\string.h C/C++ Problem
gmake: *** [SPPDemo.o] Error 1 SPPDemo C/C++ Problem
macro "_disable_interrupts" passed 1 arguments, but takes just 0 SPPDemo line 44, external location: C:\ti\ccsv6\tools\compiler\msp430_4.3.3\include\intrinsics.h C/C++ Problem
macro "_enable_interrupts" passed 1 arguments, but takes just 0 SPPDemo line 43, external location: C:\ti\ccsv6\tools\compiler\msp430_4.3.3\include\intrinsics.h C/C++ Problem
gmake: *** [BTPSKRNL.o] Error 1 SPPDemo C/C++ Problem
gmake: *** [BTPSVEND.o] Error 1 SPPDemo C/C++ Problem
gmake: *** [pre_init.o] Error 1 SPPDemo C/C++ Problem
implicit declaration of function '__va_argref' [-Wimplicit-function-declaration] BTPSKRNL.c /SPPDemo line 1246 C/C++ Problem
implicit declaration of function '__va_parmadr' [-Wimplicit-function-declaration] BTPSKRNL.c /SPPDemo line 1246 C/C++ Problem
expected identifier or '(' before '{' token SPPDemo line 148, external location: c:\ti\ccsv6\ccs_base\msp430\include_gcc\in430.h C/C++ Problem
cast from pointer to integer of different size [-Wpointer-to-int-cast] BTPSKRNL.c /SPPDemo line 1340 C/C++ Problem
macro "_get_SP_register" passed 1 arguments, but takes just 0 SPPDemo line 67, external location: C:\ti\ccsv6\tools\compiler\msp430_4.3.3\include\intrinsics.h C/C++ Problem
gmake: *** [sprintf.o] Error 1 SPPDemo C/C++ Problem
implicit declaration of function '__INTADDR__' [-Wimplicit-function-declaration] BTPSKRNL.c /SPPDemo line 258 C/C++ Problem
fatal error: SS1BTVS.h: No such file or directory BTPSVEND.c /SPPDemo line 19 C/C++ Problem
expected identifier or '(' before '{' token SPPDemo line 195, external location: c:\ti\ccsv6\ccs_base\msp430\include_gcc\in430.h C/C++ Problem
expected expression before 'char' sprintf.c /SPPDemo line 281 C/C++ Problem
implicit declaration of function '__va_parmadr' [-Wimplicit-function-declaration] sprintf.c /SPPDemo line 312 C/C++ Problem
expected identifier or '(' before '{' token SPPDemo line 241, external location: c:\ti\ccsv6\ccs_base\msp430\include_gcc\in430.h C/C++ Problem
expected expression before 'int' sprintf.c /SPPDemo line 273 C/C++ Problem
expected identifier or '(' before '{' token SPPDemo line 211, external location: c:\ti\ccsv6\ccs_base\msp430\include_gcc\in430.h C/C++ Problem
expected expression before 'int' sprintf.c /SPPDemo line 277 C/C++ Problem
expected identifier or '(' before '{' token SPPDemo line 181, external location: c:\ti\ccsv6\ccs_base\msp430\include_gcc\in430.h C/C++ Problem
expected expression before 'int' sprintf.c /SPPDemo line 267 C/C++ Problem
implicit declaration of function '__va_argref' [-Wimplicit-function-declaration] sprintf.c /SPPDemo line 261 C/C++ Problem
expected identifier or '(' before '{' token SPPDemo line 61, external location: c:\ti\ccsv6\ccs_base\msp430\include_gcc\in430.h C/C++ Problem
expected expression before 'long' sprintf.c /SPPDemo line 261 C/C++ Problem
macro "_get_interrupt_state" passed 1 arguments, but takes just 0 SPPDemo line 65, external location: C:\ti\ccsv6\tools\compiler\msp430_4.3.3\include\intrinsics.h C/C++ Problem
expected identifier or '(' before '{' token SPPDemo line 256, external location: c:\ti\ccsv6\ccs_base\msp430\include_gcc\in430.h C/C++ Problem
expected identifier or '(' before '{' token SPPDemo line 225, external location: c:\ti\ccsv6\ccs_base\msp430\include_gcc\in430.h C/C++ Problem
cast from pointer to integer of different size [-Wpointer-to-int-cast] pre_init.c /SPPDemo line 43 C/C++ Problem
cast from pointer to integer of different size [-Wpointer-to-int-cast] pre_init.c /SPPDemo line 40 C/C++ Problem
gmake: *** [MSP430_EXP5438/HAL.o] Error 1 SPPDemo C/C++ Problem
gmake: Target `all' not remade because of errors. SPPDemo C/C++ Problem
expected '=', ',', ';', 'asm' or '__attribute__' before 'void' HCITRANS.c /SPPDemo line 177 C/C++ Problem
ignoring #pragma vector [-Wunknown-pragmas] HCITRANS.c /SPPDemo line 176 C/C++ Problem
-Prashanth