Other Parts Discussed in Thread: CC2541
Hi,
I have an architecture with CC2541 as a slave connected to an external processor. I am running the full BT stack on CC2541 (not using HCI API), and running application on the external processor. I have JTAG connection to the external processor for factory image download, but don't have JTAG connection to the BT chip. My question is, what image is loaded in the BT chip before I get it? Is the image enough for me to be able to load my image from the external processor through a serial interface? If yes, is there example source code I can look at to start my development?
Thanks
Yohannes