Other Parts Discussed in Thread: CC2541, CC-DEBUGGER
Hi guys i have some beacons manufactured by Minew.
Now i will be programmer my beacons and so i have buy the TI CC Programmer and Debugger.
like you can see, on my beacon i've 5 pin (jtag connector minimal) marked with green rectangle,
so i will interface that connector with cc debugger used the minimal connection for debugg
i don't added the pull-up resistor because it's included on cc2541.
I've done a custom connector for interface of the ccdebugger with my beacons, but when i connect beacon on cc-debugger e so at my notebook, the led on my cc debugger stay on RED and in the manual this means that there is a problem in the connection or the debugger not identifies chip (it's a cc2541 soc) on my beacon.
I've done two connection test.
In the first case i've connected pin 9 (connector target of the debugger) to pin V of the beacon.
In the second test i've eliminated the connection between pin 9 and pin V and i've connected pin2 of connector target to pin V(beacon).
Iin both cases the debugger not work well, in the first case the led doesn't turn on, in the second case stay Red.
From Manual:
1)Note the concept with the target voltage sense signal. This signal is used by the level converters on the CC Debugger to handle different voltage levels on the target board and the debugger. Pin 2 on the target connector must be connected to VDD on the target board.
Where i made the mistake?