This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SmartRF Flash Programmer won't recognize dongle



Hi,

I had problem using the SmartRF Flash programmer 2 to read-back / dump out code from dongle attached.

What is the equivalent approach to perform the read-back available in SmartRF Flash programmer version1 in version 2?

At the same time, SmartRF Flash Programmer version 1 is nolonger working once version 2 is installed. Is there a workaround?

Thanks,

Christina Lim

  • Hi Christina,

    Smart RF Flash Programmer 2 only support devices using JTAG so you will have to use v1 for the dongle.
    It is fully possible to have both v1 and v2 installed at the same time as long as you don't install them to the same path.

    Regards
    Svend