This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SESUB-PAN-T2541 – treatment and transmitting PWM signal via Bluetooth

Whereas I will send a PWM signal treated in a XMC1100 microcontroller for an I/O T2541 chip. What type of internal treatment  should I do in SP13808 module to transmitting the same PWM signal via Bluetooth?

Thank you,

Ricardo

  • Hi Ricardo,
    Not sure what you are asking for here; emulating PWM over BLE does not really make sense. I guess you'd have to interpret some sort if Digital representation within a few bytes which are transmitted over the air. I think you need to read a bit about how services and characteristics are used to transfer data between two BLE devices. Google is the best place to start.

    Best Regards
    Joakim