Hello I'm building my first prototype with the CC2541 SOC and I'm in the PCB design process, I have done almost all of the connections in my schematic as the CC2541 Keyfob PDF says but I have one question I hope you can help me out with:
In the document there is a diagram about DCDC REGULATOR with the TPS62730, Can I use this to measure the level of the coin cell battery? Or this is just to supply 2.1V all the time to the CC2541 SOC? What would happen if I do not use this DCDC Regulator and I supply the CC2541 directly with the CR2032 coin battery?
If anyone has an schematic of the CC2541 in standalone mode will be very helpful for me.
Thanks