This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BTLE HCI Extension Packet Error Rate

Hi ,

 I understand that "HCI Extension Packet Error Rate" returns the following 

1. Total number of packets received,

2. Number of packets received with CRC errors

3. Number of events

4. Number of missed events

The response in BTool by calling HCI Extension Packet Error Rate" 

[182] : <Rx> - 05:02:54.492
-Type : 0x04 (Event)
-EventCode : 0xFF (HCI_LE_ExtEvent)
-Data Length : 0x0E (14) bytes(s)
Event : 0x0414 (HCIExt_PER)
Status : 0x00 (Success)
Cmd Opcode : 0xFC14 (HCIExt_PER)
Dump(Rx):

04 FF 0E 14 04 00 14 FC 01 D3 00 00 00 D5 00 02
00

Can you please tell me which one corresponds to number of packets received, no.of packets with CRC Error, no.of events,and no.of events missed?

 

Thanks and Regards,

Subha.V