Other Parts Discussed in Thread: CC2541, CC2540
I have two separate boards with different sensors, both driven by CC2541 devices. The layouts in the Bluetooth area are almost identical. Both are peripheral devices.
One board establishes a connection to Btool while the other won't.
I have attached two log files from Btool.
Board1_Log_Success.txt shows the Btool log of Board1 establishing a connection to Btool.
Board2_Log_Failure.txt shows the Btool log of Board2 failing to establish a connection to Btool.
Both logs are identical up through frame [3] (except for the board addresses and RSSI). It appears that Board2 responds with its address in frame [3], but Btool does not see Board2's GAP_DeviceInformation in frame [4] as the log of Board1 shows.
It looks like Board2's RSSI is slightly less (202 vs 206) than Board1's RSSI...
I'm assuming that the <Tx> and <Rx> notations on the Btool logs are with respect to the Btool device (ie. <Tx> shows packets that Btool has sent and <Rx> shows packets that Btool has received from the peripheral).
I'm looking for advice on how to proceed with debugging... Why would Board 2 give frame [3] but not frame [4]?
The software (except for the sensor interfaces) in the two boards is identical... The software is based on the TI peripheral device example.
Thanks!
[1] : <Tx> - 12:53:23.874 -Type : 0x01 (Command) -Opcode : 0xFE04 (GAP_DeviceDiscoveryRequest) -Data Length : 0x03 (3) byte(s) Mode : 0x03 (All) ActiveScan : 0x01 (Enable) WhiteList : 0x00 (Disable) Dump(Tx): 01 04 FE 03 03 01 00 ------------------------------------------------------------------------------------------------------------------------ [2] : <Rx> - 12:53:23.887 -Type : 0x04 (Event) -EventCode : 0xFF (HCI_LE_ExtEvent) -Data Length : 0x06 (6) bytes(s) Event : 0x067F (GAP_HCI_ExtentionCommandStatus) Status : 0x00 (Success) OpCode : 0xFE04 (GAP_DeviceDiscoveryRequest) DataLength : 0x00 (0) Dump(Rx): 04 FF 06 7F 06 00 04 FE 00 ------------------------------------------------------------------------------------------------------------------------ [3] : <Rx> - 12:53:23.987 -Type : 0x04 (Event) -EventCode : 0xFF (HCI_LE_ExtEvent) -Data Length : 0x14 (20) bytes(s) Event : 0x060D (GAP_DeviceInformation) Status : 0x00 (Success) EventType : 0x00 (Connectable Undirect Advertisement) AddrType : 0x00 (Public) Addr : 6C:EC:EB:57:42:B8 Rssi : 0xCE (206) DataLength : 0x07 (7) Data : 02:01:06:03:02:F0:FF Dump(Rx): 04 FF 14 0D 06 00 00 00 B8 42 57 EB EC 6C CE 07 02 01 06 03 02 F0 FF ------------------------------------------------------------------------------------------------------------------------ [4] : <Rx> - 12:53:24.007 -Type : 0x04 (Event) -EventCode : 0xFF (HCI_LE_ExtEvent) -Data Length : 0x2B (43) bytes(s) Event : 0x060D (GAP_DeviceInformation) Status : 0x00 (Success) EventType : 0x04 (Scan Response) AddrType : 0x00 (Public) Addr : 6C:EC:EB:57:42:B8 Rssi : 0xCD (205) DataLength : 0x1E (30) Data : 14:09:54:72:69:63:6F:72:64:65:72:54:6F:72:73:6F: 50:61:74:63:68:05:12:06:00:0C:00:02:0A:00 Dump(Rx): 04 FF 2B 0D 06 00 04 00 B8 42 57 EB EC 6C CD 1E 14 09 54 72 69 63 6F 72 64 65 72 54 6F 72 73 6F 50 61 74 63 68 05 12 06 00 0C 00 02 0A 00 ------------------------------------------------------------------------------------------------------------------------ [5] : <Rx> - 12:53:34.138 -Type : 0x04 (Event) -EventCode : 0xFF (HCI_LE_ExtEvent) -Data Length : 0x0C (12) bytes(s) Event : 0x0601 (GAP_DeviceDiscoveryDone) Status : 0x00 (Success) NumDevs : 0x01 (1) Device #0 EventType : 0x00 (Connectable Undirect Advertisement) AddrType : 0x00 (Public) Addr : 6C:EC:EB:57:42:B8 Dump(Rx): 04 FF 0C 01 06 00 01 00 00 B8 42 57 EB EC 6C ------------------------------------------------------------------------------------------------------------------------ [6] : <Tx> - 12:53:37.948 -Type : 0x01 (Command) -Opcode : 0xFE09 (GAP_EstablishLinkRequest) -Data Length : 0x09 (9) byte(s) HighDutyCycle : 0x00 (Disable) WhiteList : 0x00 (Disable) AddrTypePeer : 0x00 (Public) PeerAddr : B8:42:57:EB:EC:6C Dump(Tx): 01 09 FE 09 00 00 00 B8 42 57 EB EC 6C ------------------------------------------------------------------------------------------------------------------------ [7] : <Rx> - 12:53:37.970 -Type : 0x04 (Event) -EventCode : 0xFF (HCI_LE_ExtEvent) -Data Length : 0x06 (6) bytes(s) Event : 0x067F (GAP_HCI_ExtentionCommandStatus) Status : 0x00 (Success) OpCode : 0xFE09 (GAP_EstablishLinkRequest) DataLength : 0x00 (0) Dump(Rx): 04 FF 06 7F 06 00 09 FE 00 ------------------------------------------------------------------------------------------------------------------------ [8] : <Info> - 12:53:38.165 Device Connected Handle = 0x0000 Addr Type = 0x00 (Public) BDAddr = 6C:EC:EB:57:42:B8 ------------------------------------------------------------------------------------------------------------------------ [9] : <Rx> - 12:53:38.160 -Type : 0x04 (Event) -EventCode : 0xFF (HCI_LE_ExtEvent) -Data Length : 0x13 (19) bytes(s) Event : 0x0605 (GAP_EstablishLink) Status : 0x00 (Success) DevAddrType : 0x00 (Public) DevAddr : 6C:EC:EB:57:42:B8 ConnHandle : 0x0000 (0) ConnInterval : 0x0050 (80) ConnLatency : 0x0000 (0) ConnTimeout : 0x07D0 (2000) ClockAccuracy : 0x00 (0) Dump(Rx): 04 FF 13 05 06 00 00 B8 42 57 EB EC 6C 00 00 50 00 00 00 D0 07 00 ------------------------------------------------------------------------------------------------------------------------ [10] : <Rx> - 12:53:44.954 -Type : 0x04 (Event) -EventCode : 0xFF (HCI_LE_ExtEvent) -Data Length : 0x0B (11) bytes(s) Event : 0x0607 (GAP_LinkParamUpdate) Status : 0x00 (Success) ConnHandle : 0x0000 (0) ConnInterval : 0x000C (12) ConnLatency : 0x0000 (0) ConnTimeout : 0x03E8 (1000) Dump(Rx): 04 FF 0B 07 06 00 00 00 0C 00 00 00 E8 03 ------------------------------------------------------------------------------------------------------------------------
[1] : <Tx> - 12:55:42.036 -Type : 0x01 (Command) -Opcode : 0xFE04 (GAP_DeviceDiscoveryRequest) -Data Length : 0x03 (3) byte(s) Mode : 0x03 (All) ActiveScan : 0x01 (Enable) WhiteList : 0x00 (Disable) Dump(Tx): 01 04 FE 03 03 01 00 ------------------------------------------------------------------------------------------------------------------------ [2] : <Rx> - 12:55:42.045 -Type : 0x04 (Event) -EventCode : 0xFF (HCI_LE_ExtEvent) -Data Length : 0x06 (6) bytes(s) Event : 0x067F (GAP_HCI_ExtentionCommandStatus) Status : 0x00 (Success) OpCode : 0xFE04 (GAP_DeviceDiscoveryRequest) DataLength : 0x00 (0) Dump(Rx): 04 FF 06 7F 06 00 04 FE 00 ------------------------------------------------------------------------------------------------------------------------ [3] : <Rx> - 12:55:42.415 -Type : 0x04 (Event) -EventCode : 0xFF (HCI_LE_ExtEvent) -Data Length : 0x14 (20) bytes(s) Event : 0x060D (GAP_DeviceInformation) Status : 0x00 (Success) EventType : 0x00 (Connectable Undirect Advertisement) AddrType : 0x00 (Public) Addr : 6C:EC:EB:57:42:8F Rssi : 0xCA (202) DataLength : 0x07 (7) Data : 02:01:06:03:02:F1:FF Dump(Rx): 04 FF 14 0D 06 00 00 00 8F 42 57 EB EC 6C CA 07 02 01 06 03 02 F1 FF ------------------------------------------------------------------------------------------------------------------------ [4] : <Rx> - 12:55:52.297 -Type : 0x04 (Event) -EventCode : 0xFF (HCI_LE_ExtEvent) -Data Length : 0x0C (12) bytes(s) Event : 0x0601 (GAP_DeviceDiscoveryDone) Status : 0x00 (Success) NumDevs : 0x01 (1) Device #0 EventType : 0x00 (Connectable Undirect Advertisement) AddrType : 0x00 (Public) Addr : 6C:EC:EB:57:42:8F Dump(Rx): 04 FF 0C 01 06 00 01 00 00 8F 42 57 EB EC 6C ------------------------------------------------------------------------------------------------------------------------ [5] : <Tx> - 12:55:54.261 -Type : 0x01 (Command) -Opcode : 0xFE09 (GAP_EstablishLinkRequest) -Data Length : 0x09 (9) byte(s) HighDutyCycle : 0x00 (Disable) WhiteList : 0x00 (Disable) AddrTypePeer : 0x00 (Public) PeerAddr : 8F:42:57:EB:EC:6C Dump(Tx): 01 09 FE 09 00 00 00 8F 42 57 EB EC 6C ------------------------------------------------------------------------------------------------------------------------ [6] : <Rx> - 12:55:54.277 -Type : 0x04 (Event) -EventCode : 0xFF (HCI_LE_ExtEvent) -Data Length : 0x06 (6) bytes(s) Event : 0x067F (GAP_HCI_ExtentionCommandStatus) Status : 0x00 (Success) OpCode : 0xFE09 (GAP_EstablishLinkRequest) DataLength : 0x00 (0) Dump(Rx): 04 FF 06 7F 06 00 09 FE 00 ------------------------------------------------------------------------------------------------------------------------ [7] : <Info> - 12:56:01.333 Device Connected Handle = 0x0000 Addr Type = 0x00 (Public) BDAddr = 6C:EC:EB:57:42:8F ------------------------------------------------------------------------------------------------------------------------ [8] : <Rx> - 12:56:01.328 -Type : 0x04 (Event) -EventCode : 0xFF (HCI_LE_ExtEvent) -Data Length : 0x13 (19) bytes(s) Event : 0x0605 (GAP_EstablishLink) Status : 0x00 (Success) DevAddrType : 0x00 (Public) DevAddr : 6C:EC:EB:57:42:8F ConnHandle : 0x0000 (0) ConnInterval : 0x0050 (80) ConnLatency : 0x0000 (0) ConnTimeout : 0x07D0 (2000) ClockAccuracy : 0x00 (0) Dump(Rx): 04 FF 13 05 06 00 00 8F 42 57 EB EC 6C 00 00 50 00 00 00 D0 07 00 ------------------------------------------------------------------------------------------------------------------------ [9] : <Info> - 12:56:01.898 Device Disconnected Handle = 0x0000 Addr Type = 0x00 (Public) BDAddr = 6C:EC:EB:57:42:8F ------------------------------------------------------------------------------------------------------------------------ [10] : <Rx> - 12:56:01.898 -Type : 0x04 (Event) -EventCode : 0xFF (HCI_LE_ExtEvent) -Data Length : 0x06 (6) bytes(s) Event : 0x0606 (GAP_TerminateLink) Status : 0x00 (Success) ConnHandle : 0x0000 (0) Reason : 0x3E (Failed To Establish) Dump(Rx): 04 FF 06 06 06 00 00 00 3E ------------------------------------------------------------------------------------------------------------------------