Other Parts Discussed in Thread: CC2540
Hello everyone,
I am working in a project where the CC2540 USB dongle runs as a central and connect with three CC2540 Keyfobs at a time, every after the establish connection the central sends 14 messages request among reads and writes in every connection, before get accelerometer notifications from the keyfob.
With the first two peripherals every thing works fine, but when I connect the third keyfob, the central didn't get the response in the 12th message, the Packet Sniffer sees the response was sent from the peripheral, but somehow the central never got it.
The connection interval parameters are:
// Minimum connection interval (units of 1.25ms) (800 * 1.25ms = 1000) if automatic parameter update request is enabled
#define DEFAULT_UPDATE_MIN_CONN_INTERVAL 1600
// Maximum connection interval (units of 1.25ms) (1600 * 1.25ms = 2000) if automatic parameter update request is enabled
#define DEFAULT_UPDATE_MAX_CONN_INTERVAL 3200
// Slave latency to use if automatic parameter update request is enabled
#define DEFAULT_UPDATE_SLAVE_LATENCY 0
// Supervision timeout value (units of 10ms) if automatic parameter update request is enabled
#define DEFAULT_UPDATE_CONN_TIMEOUT 6000
Is there anyone, who can help me with this issue? I'm struggle to find a solution.
Thanks in advance,
Luiz