Other Parts Discussed in Thread: CC2640, CC2650, CC2630
Hi,
I am planning to build a proprietary wireless system with CC26XX series if possible to take a low power consumption feature of the series.
But I want to check the feasibility before I commit.
Questions,
1. Based on technical doc, application of CC2640 is limited to Bluetooth. Does this mean CC2640 can NOT be used for a proprietary system?
2. CC2650 is for multistandard, does the multistandard include a proprietary spec? Or is it limited as listed in the datasheet such as Blueetooth, ZigBee ...
3. If CC2640 is only for Bluetooth and CC2650 is for multistandard, what are the hardware difference between those two? Rough comparison of them doesn't show any difference.
4. Is there any plan to make automotive qualified product of the series?
Thanks,
Inseop