Hi,
I'm considering the CC2541 for a NON-Bluetooth application at 2.4GHz.
The cost of IAR's IDE is cost-prohibitive for me, and I am wondering:
1) For the CC2541 in proprietary (non-ble) mode, is it possible to use another IDE? Is there sample source code for using the CC2541 in proprietary mode that is known to compile and run from another IDE? If so - which one?
2) My application is basically about reading and transmitting one analog value. For an application this simple, assuming use of TI's proprietary-mode libraries for the CC2541 (and not the BLE libraries) is it likely that I could successfully use the kickstart version of IAR's embedded workbench (which is not price-prohibitive, but has a 4K size restriction)?
Thanks,
-K