Hello,
We would like to know following things for the module :
(1) BR/EDR -
- Up to 7 Active Devices
- Scatternet: Up to 3 Piconets Simultaneously, 1 as Master and 2 as Slaves
- Up to 2 SCO Links on the Same Piconet
So , is it possible we can connect - 5 Smartphone simultaneously and each can transfer and receive data.?
(2) LE Features Include:
- Support of Up to 10 Simultaneous Connections
is LE stack available ? What are the tools need to use ?
--
We like to use only SPP profile and in LE - PXP profiles.
Is these profile come already loaded into the module and needs to be done with external MCU ?
We also want secure pairing method (in which we want to keep module non-discoverable) is it possible ?
What is the connection time (Let's say device is paired first time ad for next time connections) when Smartphone enter into vicinity of the Module?
Is Bluetooth profile are available ?
Regards,
Nilesh