This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

analog on any GPIO pin of CC2640?

Other Parts Discussed in Thread: CC2640

Can the ADC or PWM functions be routed to any of the GPIO pins of the CC2640 or are some of the pins "special" and ADC can only be mapped to them?

  • Hi,

    Please see Section 12.3 "I/O Mapping and Configuration" in the CC26xx TRM (SWCU117).

    Best wishes
  • This information is also found in the datasheet.
  • JXS said:
    Please see Section 12.3 "I/O Mapping and Configuration" in the CC26xx TRM (SWCU117).

    Thanks for the answer. Just a small correction, in case someone else is looking this up, the section is 11.3.

    And just a small follow up, is mapping the output of a timer for PWM considered an analog function, and therefore only the analog capable GPIO pins can be used? 

  • pixbroker said:
    Just a small correction, in case someone else is looking this up, the section is 11.3.

    It depends on which version of the document you have. It will probably change back to 12.3 :-)

    pixbroker said:
    And just a small follow up, is mapping the output of a timer for PWM considered an analog function, and therefore only the analog capable GPIO pins can be used? 

    This is digital. I think it should be clear from the same chapter.