I am working on an application for CC2640. We are using the SmartRF06 board with the CC2650EM-71D installed. It is still early in the project, but I have some code I would like to send to someone to test. This person doesn't have code composer.
Is it possible to load code to the dev board via a utility without installing code composer? Or is it best to just download and install CCS to load the .out or .hex file?