Other Parts Discussed in Thread: CC2650
Hello all! I am currently working on a research project and we are interested in using the CC26xx for low-frequency audio sampling. Specifically, we are looking to continuously monitor sounds in the 0-4kHz range.
I was wondering two things:
(1) What kind of power consumption would I be looking at if the data was constantly streamed to a device like a smartphone? I am planning on using the same MEMs mic that is found inside the CC2650 SensorTag.
(2) Alternatively, I have considered saving the data to external flash and then "dumping" it periodically throughout the day to the device. However, if we sample at a rate of 8kHz with 16-bit resolution, this would be around 2 GB (if my calculations are correct, they might not be). Are there any type of external flash chips that are usually used with the CC26xx? I have considered lowering the resolution to 10-bits.