Other Parts Discussed in Thread: CC2650, SEGGER, CC2650EMK
The two boards in the CC2650 kit ship with pre-loaded packet error rate test software, I have two questions about that.
1) If you erase the software from the chip, is there an available .bin or .hex file to load it back on again, or once you've lost it, you've lost it. I was hoping to be able to put it back onto the board later.
2) When the packet error rate test is running on the chip I found it's just about impossible to connect to it with a Segger J-Link. The J-Link works fine after the software has been erased but fails to connect 99% of the time when it's running. Is there a reason for this? Is the board put into a hard-to-debug mode or has bits of the JTAG interface turned off or is in low-power mode or anything? Or is this a bug in the Segger driver?