Dear all:
I can not find where to call the function simpleProfileChangeCB() in BLE_Bridge project.
Can someone help me?
B.R.
KJ
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear all:
I can not find where to call the function simpleProfileChangeCB() in BLE_Bridge project.
Can someone help me?
B.R.
KJ
I used Serial_BLE_Bridge on CC2541 BoosterPack and a simple code below on MSP430F5529_LaunchPad.
I send some data on BTool, like 02:AB:CD on Handle 0x002B. (Where 01 means there are two bytes data and AB, CD are the data).
And I wrote a simple code in MSP430F5529LP to transfer data from cc2541 to PC.
// Basic MSP430 and driverLib #includes
#include "msp430.h"
//=============================================================================
void main(void)
{
WDTCTL = WDTPW | WDTHOLD; // Stop watchdog timer
P3SEL |= BIT3+BIT4; // P3.3,4 = USCI_A0 TXD/RXD
UCA0CTL1 |= UCSWRST; // **Put state machine in reset**
UCA0CTL1 |= UCSSEL_2; // SMCLK
UCA0BR0 = 9; // 1MHz 115200 (see User's Guide)
UCA0BR1 = 0; // 1MHz 115200
UCA0MCTL |= UCBRS_1 + UCBRF_0; // Modulation UCBRSx=1, UCBRFx=0
UCA0CTL1 &= ~UCSWRST; // **Initialize USCI state machine**
UCA0IE |= UCRXIE; // Enable USCI_A0 RX interrupt
P4SEL |= BIT4+BIT5; // P4.4,5 = USCI_A1 TXD/RXD
UCA1CTL1 |= UCSWRST; // **Put state machine in reset**
UCA1CTL1 |= UCSSEL_2; // SMCLK
UCA1BR0 = 9; // 1MHz 115200 (see User's Guide)
UCA1BR1 = 0; // 1MHz 115200
UCA1MCTL |= UCBRS_1 + UCBRF_0; // Modulation UCBRSx=1, UCBRFx=0
UCA1CTL1 &= ~UCSWRST; // **Initialize USCI state machine**
//UCA1IE |= UCRXIE; // Enable USCI_A1 RX interrupt
__bis_SR_register(LPM0_bits + GIE); // Enter LPM0, interrupts enabled
}
/* USCI_A0 ISR */
#pragma vector=USCI_A0_VECTOR
__interrupt void USCI_A0_ISR(void)
{
switch(__even_in_range(UCA0IV,4))
{
case 0x00: // Vector 0: No interrupts
break;
case 0x02: // Vector 2: Data received: UCRXIFG;
UCA1TXBUF = UCA0RXBUF; // Push data to TX buffer
break;
case 0x04: // Vector 4: Transmit buffer empty: UCTXIFG
break;
default:
break;
}
}
Dear Kantha,
You can try 0x002B in Handle and 02:11:22 in Value. Where "02" means 2 date fields you send.
B.R.
KJ