What are the values of the on chip load capacitors at pins X24M_N and X24M_P of the CC2650?
Reference:
CC2650 datasheet
Find, "CC2650 Application Circuit"
I see that the 24 MHz crystal used on these pins should require 5 pF to 9 pF
Reference:
CC2650 datasheet
Find, "24-MHz Crystal Oscillator (XOSC_HF)"
I assume that this 5 pF to 9 pF is not the value of the on chip load caps, since the load capacitors for the 32 kHz crystal are also specified, but they are external according to the reference designs CC2650STK and CC2650EMK where 12 pF was used.