We've been asked to design the front end of a wireless power meter. The meter takes inputs from three current transformers (CTs). The CT converts the current flowing through the "mains" to voltage. The voltage is directly proportional to the current in the "mains" line. We intend to use the CC2640 to digitize the input of 0.0 - .333V RMS from each of the CTs. The CTs have an internal impedance of 46 ohms. So, the current generated by the CTs is 0.0 - 7.0 mA.
Here's the question: Is there a way for us to use the current generated by the CTs to power an energy harvesting system capable of powering the CC2640? The three CTs tethered to a module containing little else than the CC2640 are permanently installed inside the electrical cabinet and not intended to be accessed (including to change batteries).
Thoughts?
Patrick