Hi,
I have to use internal DC to DC switcher of CC2640 and also all IO's of CC2640 on 1V8 supply voltage. I am planning to implement this as datasheet suggest that use DCDC for lowest power consumption and 1.8V for external peripherals to consume less power.
Datasheet mention that VDDS is the highest potential in the system, so can I configure CC2640 in above configuration?
Please find the below connections which I have done for same,
VDDS_DCDC= 3V
VDDS=VDDS2= 1.8V externally generated
VDDR=VDDR_RF= 1.8V output of internal dc to dc(connected to DCDC_SW through 10 uH inductor and 4.7 uF capacitor)
Thanks and regards,
Vishal