This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2540 BLUE TOOTH MODULE BLE DOES IT SUPPORT M66 OF QUECTEL WHICH HAS BUILT IN BLUE TOOTH VERSION 4 AND SUPPORTS SPP

Other Parts Discussed in Thread: CC2540

WE ARE DESIGNING BLUETOOTH USING THE CC2540 AND WOULD LIKE TO PAIR IT WITH THE M66 BLUE TOOTH , AND USE COMMANDS . PLS CONFIRM DOES THE MODULE SUPPORT OR IS THERE ANY CONVERSION.  BLE IS 4.0 VERSION AND M66 IS VERSION 3.0. 

  • Hi,

    According to this page, www.quectel.com/.../prodetail.aspx, the M66 module supports BT3.0. Bluetooth LE was not introduced until BT4.0. Since CC2540 is a single-mode BLE wireless MCU, a peer device must support BT4.0 LE at a minimum. Therefore, you cannot support a BLE connection with the M66 module.

    Please consider using a dual-mode BT device, such as a CC256x.

    Best wishes