We are currently replacing PAN1326 module with PAN1326B module which uses TI CC2564B chip. We would like to load the patch based on installed module.
I have used the command:
BTPSAPI_DECLARATION int BTPSAPI HCI_Read_Local_Version_Information(unsigned int BluetoothStackID, Byte_t *StatusResult, Byte_t *HCI_VersionResult, Word_t *HCI_RevisionResult, Byte_t *LMP_VersionResult, Word_t *Manufacturer_NameResult, Word_t *LMP_SubversionResult
I found that LMP_SubversionResult has different values for these two chips after the call. The values are 6927 for CC2564 and 7056 for CC2564B.
Can I use this to download the appropriate patches or is there a better way.
Thanks
Murshed