THis is what written in the user guide. But as I can calculate the minimum resolution for RTC is 30us. So how it can be done? Is it a mistake?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
THis is what written in the user guide. But as I can calculate the minimum resolution for RTC is 30us. So how it can be done? Is it a mistake?
So I still confuse.
As I understand the aim of the system to be in low power most of the time , that mean use the RTC as the main clock, Because the tick must run all time it should be point to the RTC as the base tick. So what is the clock the RTOS tick run on and still can be in low power?
Regards
Bar.