Dear TI team,
We have been flashing our custom built hardware around cc2650 using SmartRF06 evaluation board.
While doing so, we use external power source given to target (preferably 3V coil cell battery).
Is it possible that, this flashing can be carried without using external power source ?
(e.g. target will use internal power source, may be from evaluation board itself and in-turn derived from USB or on board)
If yes, what are the needed settings ?
Regards
Rasikraj