This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Central Scanning Data Transfer on CC2540 / CC2541

When the CC254x is in central mode and scanning I have the following questions:

1)  Are discovered peripherals having information moved from the RF core to the SoC memory via DMA or ISR?

2) Do discovered peripherals have information transferred to the SoC memory "as they are discovered" or all at 1 time in bulk at the end of a scanning window?

For example, if scanning for 100msec out of every 1 second, when does the discovered devices information get pushed into the SoC memory from the RF core?

-Marc