This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2640 advertising and scan response data

Hello,

Must the TI protocol for advertising and scan response data be adhered to in order to have the device function properly.

31 bytes are allowed for both and we are setting the data to be ascii strings.  In simple ble peripheral there is a protocol being used for both static arrays.  Furthermore, if only ascii strings are used the device does not work with ble device monitor or btool.  The protocol I am referring to is below:

// GAP - SCAN RSP data (max size = 31 bytes)
static uint8_t scanRspData[] =
{
// complete name
0x14, // length of this data
GAP_ADTYPE_LOCAL_NAME_COMPLETE,
0x53, // 'S'
0x69, // 'i'
0x6d, // 'm'
0x70, // 'p'
0x6c, // 'l'
0x65, // 'e'
0x42, // 'B'
0x4c, // 'L'
0x45, // 'E'
0x50, // 'P'
0x65, // 'e'
0x72, // 'r'
0x69, // 'i'
0x70, // 'p'
0x68, // 'h'
0x65, // 'e'
0x72, // 'r'
0x61, // 'a'
0x6c, // 'l'

// connection interval range
0x05, // length of this data
GAP_ADTYPE_SLAVE_CONN_INTERVAL_RANGE,
LO_UINT16(DEFAULT_DESIRED_MIN_CONN_INTERVAL), // 100ms
HI_UINT16(DEFAULT_DESIRED_MIN_CONN_INTERVAL),
LO_UINT16(DEFAULT_DESIRED_MAX_CONN_INTERVAL), // 1s
HI_UINT16(DEFAULT_DESIRED_MAX_CONN_INTERVAL),

// Tx power level
0x02, // length of this data
GAP_ADTYPE_POWER_LEVEL,
5 // 0dBm
};

// GAP - Advertisement data (max size = 31 bytes, though this is
// best kept short to conserve power while advertisting)
static uint8_t advertData[] =
{
// Flags; this sets the device to use limited discoverable
// mode (advertises for 30 seconds at a time) instead of general
// discoverable mode (advertises indefinitely)
0x02, // length of this data
GAP_ADTYPE_FLAGS,
DEFAULT_DISCOVERABLE_MODE | GAP_ADTYPE_FLAGS_BREDR_NOT_SUPPORTED,

// service UUID, to notify central devices what services are included
// in this peripheral
0x03, // length of this data
GAP_ADTYPE_16BIT_MORE, // some of the UUID's, but not all
#ifdef FEATURE_OAD
LO_UINT16(OAD_SERVICE_UUID),
HI_UINT16(OAD_SERVICE_UUID)
#else
LO_UINT16(SIMPLEPROFILE_SERV_UUID),
HI_UINT16(SIMPLEPROFILE_SERV_UUID)
#endif //!FEATURE_OAD
};

  • Hello Ben,

    For Advertising, you do need to set the GAP_ADTYPE_FLAGS field according to the BT Core Specification. Beyond that, you can transmit any set of bytes, up to the maximum allowed. If you do use your custom definition, other devices that do not implement this custom definition may not identify the device properly.

    Best wishes
  • Hi JXS,

    I have one more question:
    Can the advertising and scan response data be updated while the gap is up and running? So long as there is no connection and advertising is disabled. I am trying to accomplish this, but keep having a pointer be set to null in heapmgr.h. I have verified it is not an out of memory issue.

    Thanks again for your prompt reply,
    Ben