Other Parts Discussed in Thread: CC2541
Hello,
I am frequently getting a stack pointer out of range issue with my code. I would like to debug stack usage on the application task (modified simple ble peripheral task) and my UART task.
Unfortunately neither of these are showing up in the TI-RTOS Task module. They are however running because I can communicate over UART, and the app LED is running. The stack pointer issue occurs once I start doing over the air communication with the CC2541 dongle, so I'm fairly certain I have added the tasks correctly:
ICALL_MAX_NUM_TASKS=4
ICALL_MAX_NUM_ENTITIES=8
Are there other settings that need to be modified to view all tasks? I find it peculiar the application task disappeared since it was visible when I first started writing the code. Any help would be greatly appreciated!
-Ben