Dear TI Partners,
We have tried to use parameter as following,
MAX_NUM_BLE_CONNS=8
HEAPMGR_SIZE=9608
Enable HEAPMGR_METRICS
It seem could connected 7 devices, but it is not stable. Sometimes, it will be disconnection.
We have found the same device it connected twice with another handle, abnormal disconnection and scan result has connection devices.
It looks like has something problem in that.
In this case, the chip memory has used 99% (17286 bytes).
If we want to porting other function it cannot workable.
Do you have any idea about workaround or overcome for Memory and Max Connections?
Many Thanks for your help!