Other Parts Discussed in Thread: CC2540
I am using my board with CC2540, in some boards I get randomly stack over flow during debug mode or normal operation, after a while it function normally , on debug the stack overflow occurs always when i am reaching to the same I/O -P0-6(set Low).
Is there a possibility that this is a matter of HW?
I am using 3V .
This I/O controls PMOS with 100Kohm resistor between Drain to Gate.
Same issue observed when the PMOS removed.
ANLGPWR NET Connected to P0_6