I have a 2 SmartRF06EB modules with cc2650's 1 is running the HostTestApp, the other is running a modified version of the SimpleBLEPeripheral as per this tutorial: http://processors.wiki.ti.com/index.php/Tutorial:_How_to_Create_a_Custom_Bluetooth_Smart_Embedded_Application_with_the_CC2650DK
I am able to use BTool to connect, establish link, discover UUIDs and see the values just as shown in the 'Connect with BTool' portion of the tutorial. I write a 01:00 to the Client Characteristic Configuration value associated with the characteristic that is set up to be a Notification. I then increment the value from the Sunlight Sensor per the tutorial. I see the value change on the LCD, but never see the value update in BTool. If I manually read the value in BTool I see the updated value.
My understanding is that the Sunlight Sensor sends a notification when the sensor value changes, this in turn causes BTool to automatically update the value in the GUI. So what am I doing wrong, or am I misunderstanding?
Thanks for any help!