This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BLE Based message update to beacon

Other Parts Discussed in Thread: CC2540

Dear All,

                I am developing BLE message update project.I have installed the app in my android phone.I am using CR2450 N battery on my CC2540 development board.when am i entering in the app its detecting the device.IAR Embeddded workbench 8051 version 9.10.3

     first it showing the Battery information as 81%(level). its displaying message which i was given through phone to beacon.when i am updating another message beacon is showing the previous message only and battery is dry.

before inserting the battery is showing 3v,240 Amps.After updating the message is battery current 100 ma.message interval time 5 seconds.I have checked with the faulty battery on another beacon.its not working.battery is full dry.

My question is where will be the mistake happened on software or hardware.

  • Hello,

    It's hard to tell from the description. What does "full dry" mean? You are using a CR2450 batt, which has a higher rated capacity than the standard CR2032 batteries. Which CC2540 dev board are you using?

    Best wishes