This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Using CC2592 Front End with CC2541 in proprietary mode?

Other Parts Discussed in Thread: CC2590

Hi,

In section-8 of Application note SWRA422, 3 steps mentioned to have automatic control of CC2592:
1- The specific pins on CC2541 be connected to control pins of cc2592: This is match with our design
2- the registers listed in Table 8.2 need to be changed from the recommended CC2541 settings to control the CC2590and give optimum performance: I did that.
3- use of HCI_EXT_ExtendRFRangeCmd. This command is used to configure the CC254x to automatically control the CC2590: I am using the only available code for cc2541 proprietary and it does not have HCI_EXT_ExtendRFRangeCmd function. Where this function should be found and if it is for BLE how it should be integrated to proprietary mode?

Thank you,
Amir