This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Read and write characteristic CC2541



Hi all,

    Can anyone please suggest me  which function to process the characteristic value when central device writes to characteristic. i know SimpleProfile_GetParameter() is used to read the characteristic value in simplebelperipheral project. I want little flow of the process.  Do i need to process in  case SIMPLEPROFILE_CHAR1: of static void simpleProfileChangeCB( uint8 paramID ) for characteristic1? Through BTOOL and mobile app i have tested to write and read characteristic but i want to know where can i add my code to process it?


Thanks