This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2650 CC-DEVPACK-DEBUG Connections

Other Parts Discussed in Thread: CC2650

Hello,

I am working on a project where I want to connect the CC2650 to additional sensors.  I see three ways to do this:

1. Find a prototyping board or cable that has an LSS-110-01-F-DV-A-TR on it that would allow connectivity to a breadboard or some other connector that would make it easier to access hand soldered components.

2. Solder a set of vertical pins into the test points on the CC-DEVPACK-DEBUG and use that to connect to a breadboard through a cable that terminates in some breadboard friendly connector.

3. Direct solder wires to the test points or grove connectors that are unpopulated on the CC-DEVPACK-DEBUG.

A couple of questions:

1. Has anyone found a prototyping board or cable with an LSS-110-F-DV-A-TR on it?

2. The schematics for the CC-DEVPACK-DEBUG list under the test points a part number of FTS-110-02-L-D.  There is a bit of confusion on the Internet when you look up this part number.  SAMTEK the manufacturer states that the -02 model is 1.91mm pitch while distributors have it listed as 1.27mm pitch.  Measuring the test points they appear to be 1.27mm.  Has anyone verified that they are 1.27mm?

Thanks,

digitalhack