This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Throughout speed about CC26XX



Hi,

Currently, I am working on CC26XX, and I have some question to ask:

1. What's the max throughout speed between CC26XX and CC26XX, and what's max speed between  cc26xx and mobile phone? Do you have any testing on that, If have, could you share them for me?

As we know, BLE transmit interval between 7.5ms~4s, and for every transmit, 20bytes is max. That means the theory max speed is 20bytes/7.5ms=2.67kbytes/s, is that right?  In my pre-product, I use nrf51822, it can transmit 6 packs between one intreval, that means 20bytes*6/7.5ms=16kbytes/s.

2. Could cc26xx support private protocal stack? And if use private protocal stack, what max speed can be reach, and what can I do to start? Is there any private protocal stack demo to be share?

thanks.