Other Parts Discussed in Thread: CC2640
Hi,
I'm new to cc2640, right now I'm working on the UART reading function. I've initiated it and opened it with the function UART_Open(), and then I use UART_read() but can get nothing. I print message inner the readcallback function, but I find that this function doesn't work. Please help. Thanks!
I copy the code here, please check:
// Configure UART parameters.
UART_Params_init(¶ms);
params.baudRate = 115200;
params.readDataMode = UART_DATA_BINARY;
params.writeDataMode = UART_DATA_BINARY;
params.dataLength = UART_LEN_8;
params.stopBits = UART_STOP_ONE;
params.readMode = UART_MODE_CALLBACK;
params.writeMode = UART_MODE_CALLBACK;
params.readReturnMode = UART_RETURN_FULL;//UART_RETURN_NEWLINE;//UART_RETURN_FULL;
params.readEcho = UART_ECHO_OFF;
params.readTimeout = BIOS_WAIT_FOREVER;
#if (UART_CALL_BACK ==1)
params.readCallback = Uart_ReadCallback;
params.writeCallback = Uart_WriteCallback;
#else
params.readCallback = NULL;
params.writeCallback = NULL;
#endif
uartHandle = UART_open(Board_UART, ¶ms);
print_msg("UART open: Baudrate = %d \r\n", params.baudRate);
UART_control(uartHandle, UARTCC26XX_RETURN_PARTIAL_ENABLE, NULL);
int rxBytes = UART_read(uartHandle, Uart_RxBuf, UART_FIFO_FULL_SIZE);
print_msg("#1 UART read %d bytes = %d \r\n", rxBytes);
-------------------------------------------------------------------------------------------------------------------------------
// Callback function
void Uart_ReadCallback(UART_Handle handle, void *rxBuf, size_t size)
{
//dubug
print_msg("#uart read callback \r\n");
// Copy bytes from RX buffer to TX buffer
for (size_t i = 0; i < size; i++) {
Uart_TxBuf[i] = ((uint8_t *)rxBuf)[i];
}
// Echo the bytes received back to transmitter
UART_write(handle, Uart_TxBuf, size);
// Start another read, with size the same as it was during first call to UART_read()
UART_read(handle, Uart_RxBuf, UART_FIFO_FULL_SIZE);
//dubug
PUTchar8x16(1<<1, 2, (unsigned char *)Uart_TxBuf, 0);
print_msg("\r\n");
}