Hi,
The CC2640 and CC1310 device has three package options.
RSM (QFN32) ,RHB (QFN32) & RGZ (QFN48)...from CC2640 datasheet.
Does all the packages support all the Serial interfaces(I2C,SPI & I2S)?
We would like to know if we could choose RHB (QFN32) package
for the below requirement.
SPI: 1 Channel(4 I/O ports)
I2C: 1 Channel(2 I/O ports)
Input: 4 I/O ports
Output: 5 I/O ports
Total: 15 I/O ports
As per the datasheet, the RHB package has 15 GPIO.
But it is not clear that all the 15 ports are availabe and
is it possible to implement both SPI and I2C in RHB Package?
And will this be same for CC1310 series?
The Manual(SWCU117B) Table 11-2 has a note saying "CC13xx does not have DIO0"
does it mean CC1310's RHB package has only 14 GPIO?
Best Regards
Kummi