Hello
Is anyone else having problems with the com ports and the CC-DEVPACK-DEBUG? Anyone know of a solution?
- Disconnect the CC-DEVPACK-DEBUG from the USB cable while a software application still has the com port opened.
- Reconnect the CC-DEVPACK-DEBUG to the USB cable
The com port ends up in a state:
- Where no data shows up in the software application that has the com port opened.
- If you close the port in the application and try and reopen it you get an error that the port doesn't exist.
- You have to reboot to be able to use the com port again.
I am using CCS 6.1.00104 and the have the 1.6 XDS110 drivers loaded on Windows 7 64 bit.
Thanks,
digitalhack