This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

cc2540 minimum connection based code download using Smart RF studio.

Other Parts Discussed in Thread: CC2540

Hi All, 

Can you please tell me how to download hex code into the CC2540 IC using minimum debug configuration.

I have DC, DD, Reset, VCC, GND all connected.

I saw voltage of 1.25V at the R bias pin IC.30 pin.

I saw voltage of 1.8V at IC.40 pin.

I tried to connect the board using CC Debugger, but the debugger is not able to detect the IC.

Question:

Is it possible for code download using Smart RF Flash Programmer to download code into the CC2540 IC using the CC Debugger?

  • If your CC debugger can not detect your CC254x, I suggest you to check CC254x crystal circuit. If CC debugger can detect CC254x, it is no problem to use Flash Programmer to download code into CC2540 by CC debugger.