Hello
We need support in deciding the Cbuf value of TPS62730. In our circuit we interface TPS62730 with CC2541. We are using Lithium polycarbon monofluoride battery(3V) and our Tx duration is 1sec for each 5sec. We will consume approximately 18mA during Tx. Since the battery chemistry of the coin cell we use doesn't fall under any of the battery chemistry listed in the datasheet (Li-SOCl2, Li-SO2, Li-MnO2) we need help in getting the correct value for Cbuf. Any help is very much appreciated.
-Vipin